BDB_bOutOfBandCommissionGetKey#
bool_tBDB_bOutOfBandCommissionGetKey(
uint8* pu8InstallCode,
uint8* pu8EncKey,
uint64 u64ExtAddress,
uint8* pu8DecKey,
uint8* pu8Mic);
Description#
This function is used to decrypt an encrypted security key. It may be used to decrypt the network key received from another device during out-of-band commissioning.
The function requires the install code that was used to generate the pre-configured link key used to encrypt the key.
For an overview of out-of-band commissioning, refer to Out-Of-Band Commissioning.
Parameters#
pu8InstallCode: Pointer to install code used to generate the pre-configured link key used in the encryption.
pu8EncKey: Pointer to encrypted key.
u64ExtAddress: Pointer to IEEE/MAC address of originating device.
pu8DecKey: Pointer to location to receive the decrypted key.
pu8Mic: Pointer to the MIC value to be used to validate the decryption.
Returns#
TRUE if key successfully decrypted, otherwise FALSE
Parent topic:Functions