MCUXpresso SDK Documentation

ZPS_vSetOverrideLocalIeeeAddr

ZPS_vSetOverrideLocalIeeeAddr#

void ZPS_vSetOverrideLocalIeeeAddr(
                    uint64 *pu64Address);

Description#

This function can be used to over-ride the 64-bit IEEE (MAC) address of the device where this address is stored locally in the index sector of Flash memory.

Note: If required, this function must be called before the ZigBee PRO stack is initialized.

Parent topic:ZPS_vSetOverrideLocalIeeeAddr

Parameters#

pu64Address Pointer to the 64-bit IEEE MAC address

Note: The stack stores a pointer to pu64Addressand does not take a copy of the address. The memory pointed to by pu64Address must therefore be static or constant, and must not be on the CPU stack.

Parent topic:ZPS_vSetOverrideLocalIeeeAddr

Parent topic:Addressing functions