ZPS_vAplSecSetInitialSecurityState
ZPS_teStatus ZPS_vAplSecSetInitialSecurityState(
ZPS_teZdoNwkKeyState eState,
uint8 *pu8Key,
uint8 u8KeySeqNum
ZPS_teApsLinkKeyType eKeyType);
Description
This function is used to configure the initial state of ZigBee security on the local node. This requires a security key to be specified that is used in setting up network-level security.
Note: Before using this function, security must be enabled on the node via the device parameter Security Enabled in the ZPS Configuration Editor.
You must provide a pointer to an initial link key of one of the following types:
Pre-configured global link key
Pre-configured unique link key
These key types are described in Section 6.8.2. The network key randomly generated by the Trust Centre is communicated to the local node in encrypted form using the specified link key.
Parameters
eState: The state of the link key, one of:
ZPS_ZDO_PRECONFIGURED_LINK_KEY
ZPS_ZDO_ZLL_LINK_KEY
pu8Key: Pointer to pre-configured link key
u8KeySeqNum: Not used when specifying a link key - ignore this parameter
eKeyType: Type of link key, one of:
ZPS_APS_UNIQUE_LINK_KEY
ZPS_APS_GLOBAL_LINK_KEY
Parent topic:ZPS_vAplSecSetInitialSecurityState
Returns
ZPS_E_SUCCESS (security state successfully initialized)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_vAplSecSetInitialSecurityState
Parent topic:Security functions