MCUXpresso SDK Documentation

ZPS_u64GetFlashMappedIeeeAddress

ZPS_u64GetFlashMappedIeeeAddress#

uint64 ZPS_u64GetFlashMappedIeeeAddress(
                    uint16 u16Location);

Description#

This function can be used on the Trust Centre to obtain the 64-bit IEEE (MAC) address of the node for which a link key has been persistently stored in the specified location in devices Flash memory. The location is specified as the number of the array element for the node - see the description of ZPS_vTcInitFlash.

Parent topic:ZPS_u64GetFlashMappedIeeeAddress

Parameters#

u16Location: Number of the array element for the node

Parent topic:ZPS_u64GetFlashMappedIeeeAddress

Returns#

64-bit IEEE/MAC address obtained.

Parent topic:ZPS_u64GetFlashMappedIeeeAddress

Parent topic:Addressing functions