MCUXpresso SDK Documentation

ZPS_tsInterPanAddress

ZPS_tsInterPanAddress#

This structure is used to specify the destination for an inter-PAN transmission. The ZPS_tsInterPanAddressstructure is detailed below.

typedef struct
{
    enum {
        ZPS_E_AM_INTERPAN_GROUP = 0x01,
        ZPS_E_AM_INTERPAN_SHORT,
        ZPS_E_AM_INTERPAN_IEEE
    }eMode;
    uint16 u16PanId;
    ZPS_tuAddress uAddress;
} ZPS_tsInterPanAddress;

where:

  • eModeis used to specify the type of destination address that will be used in the field uAddressbelow. One of the following enumerations must be specified:

    • ZPS_E_AM_INTERPAN_GROUP indicates that a 16-bit group address will be used to specify multiple target nodes in the destination network (the group address must be valid in the destination network)

    • ZPS_E_AM_INTERPAN_SHORT indicates that a 16-bit network/short address will be used to specify a single target node or a broadcast to all nodes in the destination network

    • ZPS_E_AM_INTERPAN_IEEE indicates that a 64-bit IEEE/MAC address will be used to specify a single target node in the destination network

  • u16PanIdis the PAN ID of the destination network - a value 0xFFFF can be used to specify a broadcast to all reachable ZigBee PRO networks

  • uAddressis the address of the target node(s) in the destination network (the address type must be as specified above in the eModefield) - a value of 0xFFFF can be used to specify a broadcast to all nodes in the destination network(s).

Parent topic:Other structures