ZPS_tsAplZdpUserDescSet#
This structure is used by the function ZPS_eAplZdpUserDescSetRequest(). It represents a request used to configure the User descriptor on a remote node.
The ZPS_tsAplZdpUserDescSetstructure is detailed below.
typedef struct {
uint16 u16NwkAddrOfInterest; uint8 u8Length;
char szUserDescriptor[ZPS_ZDP_LENGTH_OF_USER_DESC];
} ZPS_tsAplZdpUserDescSet;
where:
u16NwkAddrOfInterestis the network address of the node of interestu8Lengthis the length of the User descriptorszUserDescriptoris the new User descriptor for the remote node as a character array.
Parent topic:ZDP Request structures