ZPS_tsAplZdpSystemServerDiscoveryReq
This structure is used by the ZPS_eAplZdpSystemServerDiscoveryRequest() function. It represents a request for information on the available services of a remote node.
The ZPS_tsAplZdpSystemServerDiscoveryReqstructure is detailed below.
typedef struct {
uint16 u16ServerMask;
} ZPS_tsAplZdpSystemServerDiscoveryReq;
where u16ServerMaskis a bitmask representing the required services (1 for ‘required’, 0 for ‘not required’). This bitmask is detailed in the table below.
Services Bitmask
Bit |
Service |
|---|---|
0 |
Primary Trust Centre |
1 |
Backup Trust Centre |
2 |
Primary Binding Table Cache |
3 |
Backup Binding Table Cache |
4 |
Primary Discovery Cache |
5 |
Back-up Discovery Cache |
6 |
Network Manager |
7-15 |
Reserved |
Parent topic:ZDP Request structures