ZPS_tsAplZdpSimpleDescStoreReq
This structure is used by the function ZPS_eAplZdpSimpleDescStoreRequest(). It represents a request to a remote node to store the Simple descriptor of one of the local node’s endpoints.
The ZPS_tsAplZdpSimpleDescStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr; uint8 u8Length;
/* Rest of message is variable length */ ZPS_tsAplZdpSimpleDescType sSimpleDescriptor;
} ZPS_tsAplZdpSimpleDescStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodeu8Lengthis the length of the Simple descriptor to storesSimpleDescriptoris a pointer to the Simple descriptor to store (this is itself a structure of the typeZPS_tsAplZdpSimpleDescType, detailed in Section8.2.1.3)
Parent topic:ZDP Request structures