ZPS_tsAplZdpPowerDescStoreReq
This structure is used by the function ZPS_eAplZdpPowerDescStoreRequest(). It represents a request to a remote node to store the Power descriptor of the local node.
The ZPS_tsAplZdpPowerDescStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
/* Rest of message is variable length */ ZPS_tsAplZdpNodePowerDescriptor sPowerDescriptor;
} ZPS_tsAplZdpPowerDescStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodesPowerDescriptoris a pointer to the Power descriptor to store (this is itself a structure of the typeZPS_tsAplZdpNodePowerDescriptor, detailed in Section8.2.1.2)
Parent topic:ZDP Request structures