MCUXpresso SDK Documentation

ZPS_tsAplZdpNwkAddrReq

ZPS_tsAplZdpNwkAddrReq#

This structure is used by the function ZPS_eAplZdpNwkAddrRequest(). It represents a request for the network address of the node with a given IEEE address.

The ZPS_tsAplZdpNwkAddrReqstructure is detailed below.

typedef struct {
  uint64 u64IeeeAddr;
  uint8 u8RequestType;
  uint8 u8StartIndex;
} ZPS_tsAplZdpNwkAddrReq;

where:

  • u64IeeeAddr is the IEEE address of the node of interest.

  • u8RequestType is the type of response required:

    • 0x00: Single device response, which contains only the network address of the target node.

    • 0x01: Extended response, which also includes the network addresses of neighboring nodes.

    • All other values are reserved.

  • u8StartIndex is the Neighbor table index of the first neighboring node to be included in the response, if an extended response has been selected.

Parent topic:ZDP Request structures