MCUXpresso SDK Documentation

ZPS_tsAplZdpMgmtNwkDiscReq

ZPS_tsAplZdpMgmtNwkDiscReq#

This structure is used by the function ZPS_eAplZdpMgmtNwkDiscRequest(). It represents a request to a remote node to discover any other wireless networks that are operating in the neighborhood.

The ZPS_tsAplZdpMgmtNwkDiscReqstructure is detailed below.

typedef struct {
 uint32 u32ScanChannels;
 uint8 u8ScanDuration;
 uint8 u8StartIndex;
} ZPS_tsAplZdpMgmtNwkDiscReq;

where:

  • u32ScanChannelsis a bitmask of the radio channels to scan (‘1’ means scan, ‘0’ means do not scan):

    • Bits 0 to 26 respectively represent channels 0 to 26 (only bits 11 to 26 are relevant to the 2400-MHz band)

    • Bits 27 to 31 are reserved

  • u8ScanDurationis a value in the range 0x00 to 0x0E that determines the time spent scanning each channel - this time is proportional to 2u8ScanDuration+1

  • u8StartIndexis the index of the first result from the results list to include in the response to this request

Parent topic:ZDP Request structures