ZPS_tsAplZdpMgmtLeaveReq
This structure is used by the function ZPS_eAplZdpMgmtLeaveRequest(). It requests a remote node to leave the network.
The ZPS_tsAplZdpMgmtLeaveReqstructure is detailed below.
typedef struct {
uint64 u64DeviceAddress;
uint8 u8Flags;
} ZPS_tsAplZdpMgmtLeaveReq;
where:
u64DeviceAddressis the IEEE address of the device being asked to leave the network.u8Flagsis an 8-bit bitmap containing the following flags:Rejoin flag (bit 0): Set to 1 if the node requested to leave the network should immediately try to rejoin the network, otherwise set to 0.
Remove Children flag (bit 1): Set to 1 if the node requested to leave the network should also request its own children (if any) to leave the network, otherwise set to 0.
Reserved (bits 7-2).
Parent topic:ZDP Request structures