MCUXpresso SDK Documentation

ZPS_tsAplZdpFindNodeCacheReq

ZPS_tsAplZdpFindNodeCacheReq#

This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to search for nodes in the network that hold ‘discovery information’ about a particular node.

The ZPS_tsAplZdpFindNodeCacheReqstructure is detailed below.

typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpFindNodeCacheReq;

where:

  • u16NwkAddris the network address of the node of interest

  • u64IeeeAddris the IEEE address of the node of interest

Parent topic:ZDP Request structures