ZPS_tsAplZdpExtendedSimpleDescReq
This structure is used by the **ZPS_eAplZdpExtendedSimpleDescRequest()**function. It represents a request for the Simple descriptor of an endpoint on the node with a given network address. This request is required when the endpoint has more input/output clusters than the usual ZPS_eAplZdpSimpleDescRequest() function can deal with.
The ZPS_tsAplZdpExtendedSimpleDescReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint8 u8EndPoint;
uint8 u8StartIndex;
} ZPS_tsAplZdpExtendedSimpleDescReq;
where:
u16NwkAddrOfInterestis the network address of the node of interestu8EndPointis the number of the relevant endpoint on the node (1-240)u8StartIndexis the index of the first cluster of interest in the input and output cluster lists for the endpoint (this and subsequent clusters will be reported in the response)
Parent topic:ZDP Request structures