ZPS_tsAplZdpDiscoveryCacheReq#
This structure is used by the function ZPS_eAplZdpDiscoveryCacheRequest(). It represents a request to find the nodes in the network which have a primary discovery cache.
The ZPS_tsAplZdpDiscoveryCacheReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
} ZPS_tsAplZdpDiscoveryCacheReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending node
Parent topic:ZDP Request structures