ZPS_tsAplZdpBindRegisterReq
This structure is used by the function ZPS_eAplZdpBindRegisterRequest(). It represents a request to inform a remote node with a primary binding table cache that the local node will hold its own Binding table entries.
The ZPS_tsAplZdpBindRegisterReqstructure is detailed below.
typedef struct {
uint64 u64NodeAddress;
} ZPS_tsAplZdpBindRegisterReq;
where u64NodeAddressis the IEEE address of the local node.
Parent topic:ZDP Request structures