ZPS_tsAplZdpBackupBindTableReq
This structure is used by the function ZPS_eAplZdpBackupBindTableRequest(). It represents a request to a remote node to save a back-up of the local primary binding table cache (whole or in part).
The ZPS_tsAplZdpBackupBindTableReqstructure is detailed below.
typedef struct {
uint16 u16BindingTableEntries;
uint16 u16StartIndex;
uint16 u16BindingTableListCount;
/* Rest of message is variable length */
ZPS_tsAplZdpBindingTable sBindingTable;
} ZPS_tsAplZdpBackupBindTableReq;
where:
u16BindingTableEntriesis the total number of entries in the primary binding table cache.u16StartIndexis the binding table index of the first entry to be backed up.u16BindingTableListCountis the number of binding table entries in the list to be backed up (sBindingTable).sBindingTableis a pointer to the list of binding table entries to be backed up. Each list item is of the typeZPS_tsAplZdpBindingTabledetailed below:
ZPS_tsAplZdpBindingTable
typedef struct
{
uint64 u64SourceAddress;
ZPS_tsAplZdpBindingTableEntry* psBindingTableEntryForSpSrcAddr;
}ZPS_tsAplZdpBindingTable;
where:
u64SourceAddressis the IEEE source address for the binding table entry.psBindingTableEntryForSpSrcAddris the binding table entry. This is of the typeZPS_tsAplZdpBindingTableEntrydetailed below.
ZPS_tsAplZdpBindingTableEntry
typedef struct
{
uint16 u16ClusterId;
uint8 u8SourceEndpoint;
uint8 u8DstAddrMode;
union {
struct {
uint16 u16DstAddress;
} sShort;
struct {
uint64 u64DstAddress;
uint8 u8DstEndPoint;
} sExtended;
};
}ZPS_tsAplZdpBindingTableEntry;
where:
u16ClusterIdis the ID of the cluster (on the local endpoint) for the bindingu8SrcEndpointis the number of the source endpoint for the binding (1-240)u8DstAddrModeis the destination addressing mode for remaining elements (see Table below)u16DstAddressis the address the destination node for the binding (address type according to setting ofu8DstAddrMode)u8DstEndPointis the number of the destination endpoint for the binding (1-240)
Addressing modes
u8DstAddrMode |
Code |
Description |
|---|---|---|
0x01 |
ZPS_E_ADDR_MODE_GROUP |
16-bit Group address |
0x03 |
ZPS_E_ADDR_MODE_IEEE |
64-bit IEEE/MAC address |
Parent topic:ZDP Request structures