ZPS_tsAplZdpActiveEpStoreReq
This structure is used by the function ZPS_eAplZdpActiveEpStoreRequest(). It represents a request to a remote node to store the list of active endpoints of the local node.
The ZPS_tsAplZdpActiveEpStoreReqstructure is detailed below.
typedef struct { uint16 u16NwkAddr; uint64 u64IeeeAddr;
uint8 u8ActiveEPCount;
/* Rest of message is variable length */ uint8* pu8ActiveEpList;
} ZPS_tsAplZdpActiveEpStoreReq;
where:
u16NwkAddris the network address of the sending nodeu64IeeeAddris the IEEE address of the sending nodeu8ActiveEPCountis the number of active endpoints in the list to storepu8ActiveEpListis a pointer to the list of active endpoints to store
Parent topic:ZDP Request structures