ZPS_tsAplApsKeyDescriptorEntry
This structure contains a link key for secured communications with another node.
typedef struct
{
uint32 u32OutgoingFrameCounter;
uint16 u16ExtAddrLkup;
uint8 au8LinkKey[ZPS_SEC_KEY_LENGTH];
} ZPS_tsAplApsKeyDescriptorEntry;
where:
u32OutgoingFrameCounteris the outgoing frame counter value which is incremented on each transmission to a destination address below.u16ExtAddrLkupis the index of the local look-up table entry that contains the IEEE/MAC address of either the Trust Centre or the target node.au8LinkKey[]is an array containing the link key.
Parent topic:Other structures