MCUXpresso SDK Documentation

ZPS_tsAfProfileDataReq

ZPS_tsAfProfileDataReq#

This structure is used to specify the transmission details for a data transmission submitted using the function ZPS_eAplAfApsdeDataReq().

The ZPS_tsAfProfileDataReqstructure is detailed below.

typedef struct {
    ZPS_tuAddress             uDstAddr;
    uint16                    u16ClusterId;
    uint16                    u16ProfileId;
    uint8                     u8SrcEp;
    ZPS_teAplApsdeAddressMode eDstAddrMode;
    uint8                     u8DstEp;
    ZPS_teAplAfSecurityMode   eSecurityMode;
    uint8                     u8Radius;
}ZPS_tsAfProfileDataReq;

where:

  • uDstAddris the address of the destination node for the transmission request (can be 16- or 64-bit, as specified by eDstAddrMode).

  • u16ClusterIdis the Cluster ID of the destination cluster.

  • u16ProfileIdis the Profile ID of the destination application profile.

  • u8SrcEpis the source endpoint number (1-240) on the local node.

  • eDstAddrModeis the type of destination address, one of (also see the table, Table):

    • ZPS_E_ADDR_MODE_BOUND (no address needed for bound nodes).

    • ZPS_E_ADDR_MODE_GROUP (16-bit group address).

    • ZPS_E_ADDR_MODE_SHORT (16-bit network address).

    • ZPS_E_ADDR_MODE_IEEE (64-bit IEEE/MAC address).

  • u8DstEpis the destination endpoint number (1-240) on the remote node.

  • eSecurityModeis the security mode for the data transfer, one of:

    • ZPS_E_APL_AF_UNSECURE (no security enabled)

    • ZPS_E_APL_AF_SECURE (Application-level security using link key and network key)

    • ZPS_E_APL_AF_SECURE_NWK (Network-level security using network key)

    • ZPS_E_APL_AF_SECURE | ZPS_E_APL_AF_EXT_NONCE (Application-level security using link key and network key with the extended NONCE included in the frame)

    • ZPS_E_APL_AF_WILD_PROFILE (May be combined with the above flags using OR operator. Sends the message using the wildcard profile (0xFFFF) instead of the profile in the associated Simple descriptor).

  • u8Radiusis the maximum number of hops permitted to the destination node (zero value specifies that default maximum is to be used).

Parent topic:Other structures