MCUXpresso SDK Documentation

ZPS_tsAfPollConfEvent

ZPS_tsAfPollConfEvent#

This structure is used in the ZPS_EVENT_NWK_POLL_CONFIRM event, which reports the completion of a poll request sent from the (local) End Device to its parent.

The ZPS_tsAfPollConfEventstructure is detailed below.

typedef struct {
    uint8 u8Status;
} ZPS_tsAfPollConfEvent;

where u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

Parent topic:Event structures