ZPS_tsAfNwkJoinedEvent#
This structure is used in the events ZPS_EVENT_NWK_JOINED_AS_ROUTER and ZPS_EVENT_NWK_JOINED_AS_ENDDEVICE, which confirm that the local device (Router or End Device) has successfully joined a network.
The ZPS_tsAfNwkJoinedEventstructure reports the network address that the parent has assigned to the new node and is detailed below.
typedef struct
{
uint16 u16Addr;
bool_t bRejoin;
} ZPS_tsAfNwkJoinedEvent;
where:
u16Addris the 16-bit network address allocated to the joining node.bRejoinindicates whether the join was a rejoin (TRUE) or a new association (FALSE).
Parent topic:Event structures