MCUXpresso SDK Documentation

ZPS_tsAfInterPanDataConfEvent

ZPS_tsAfInterPanDataConfEvent#

This structure is used in the ZPS_EVENT_APS_INTERPAN_DATA_CONFIRM event, which indicates that an inter-PAN communication has been sent by the local node and an acknowledgment has been received from the first hop node (this acknowledgment is not generated in the case of a broadcast).

The ZPS_tsAfInterPanDataConfEventstructure is detailed below.

typedef struct {
    uint8 u8Status;
    uint8 u8Handle;
} ZPS_tsAfInterPanDataConfEvent;

where

  • u8Statusis one of the status codes from the lower stack layers, detailed in Section 11.2.

  • u8Handleis a handle for internal use.

Parent topic:Event structures