ZPS_TclkDescriptorEntry
This structure is used on the Trust Centre to hold information in RAM about a link key for a node, where this link key is held in persistent storage in devices Flash memory, as enabled by the function ZPS_vTcInitFlash(). If this feature is used, the application must allocate space for an array of these structures in RAM, with one structure for each potential node in the network.
typedef struct
{
uint16 u16CredOffset;
uint16 u16TclkRetries;
} ZPS_TclkDescriptorEntry;
where:
u16CredOffsetis the offset, in bytes, of the storage location for the node’s link key in the relevant Flash memory sector.u16TclkRetriesis the number of retries that were attempted to negotiate the link key between the Trust Centre and the node.
Parent topic:Other structures