MCUXpresso SDK Documentation

ZPS_psNwkNibGetHandle

ZPS_psNwkNibGetHandle#

ZPS_tsNwkNib *ZPS_psNwkNibGetHandle(void *pvNwk);

Description#

This function obtains a handle for the NIB (Network Information Base) corresponding to the specified NWK layer instance.

The function should be called after ZPS_pvAplZdoGetNwkHandle(), which is used to obtain a pointer to the NWK layer instance.

The NIB is detailed in the ZigBee Specification (05347) from the ZigBee Alliance. This function is not strictly a ZDO function.

Parent topic:ZPS_psNwkNibGetHandle

Parameters#

pvNwk Pointer to NWK layer instance

Parent topic:ZPS_psNwkNibGetHandle

Returns#

Pointer to NIB structure

Parent topic:ZPS_psNwkNibGetHandle

Example#

void *pvNwk; = ZPS_pvAplZdoGetNwkHandle();
 ZPS_tsNwkNib *pNib = ZPS_psNwkNibGetHandle(pvNwk);

Parent topic:ZPS_psNwkNibGetHandle

Parent topic:Object Handle functions