ZPS_eAplZdpRecoverSourceBindRequest
ZPS_teStatus ZPS_eAplZdpBackupSourceBindRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpBackupSourceBindReq
*psZdpBackupSourceBindReq);
Description
This function requests that a back-up of the locally held source binding table is recovered from a remote node. The function must be called from a node with a primary binding table cache and the destination node of the request must hold the corresponding back-up binding table cache.
Note: This function is provided in the NXP ZDP API for the reason of interoperability with nodes running non-NXP ZigBee PRO stacks that support the generated request. On receiving a request from this function, the NXP ZigBee PRO stack will return the status ZPS_ZDP_NOT_SUPPORTED.
This request must indicate the starting index in the binding table for the recovery. The request is represented by the structure below (further detailed in Section 9.2.2.32).
typedef struct {
uint16 u16StartIndex;
} ZPS_tsAplZdpRecoverSourceBindReq;
The remote node replies with a Recover_Source_Bind_rsp response containing the required binding table entries, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpRecoverSourceBindRsp(detailed in Section 9.2.3.32). As many binding entries as possible are included in this response. If the returned binding table is incomplete, this is indicated in the response and this function must be called again, with the appropriate starting index, to recover the rest of the table.
Parent topic:ZPS_eAplZdpRecoverSourceBindRequest
Parameters
hAPduInst Handle of APDU instance in which request is sent.
uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpRecoverSourceBindReq Pointer to request (see above)
Parent topic:ZPS_eAplZdpRecoverSourceBindRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpRecoverSourceBindRequest
Parent topic:Binding functions