ZPS_eAplZdpMgmtNwkUpdateRequest
ZPS_teStatus ZPS_eAplZdpMgmtNwkUpdateRequest(
PDUM_thAPduInstance hAPduInst,
ZPS_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS_tsAplZdpMgmtNwkUpdateReq
*psZdpMgmtNwkUpdateReq);
Description
This function requests an update of network parameters related to radio communication. The request can specify any of the following:
update the radio channel mask (for scans) and the 16-bit network address of the network manager (node nominated to manage radio-band operation of network)
change the radio channel used
scan radio channels and report the results
The request can be broadcast or unicast to nodes with radio receivers that are configured to remain on during idle periods.
The request is represented by the structure below (further detailed in Section9.2.2.41).
typedef struct {
uint32 u32ScanChannels;
uint8 u8ScanDuration;
uint8 u8ScanCount;
uint8 u8NwkUpdateId;
uint16 u16NwkManagerAddr;
} ZPS_tsAplZdpMgmtNwkUpdateReq;
The specific action to be taken as a result of this request is indicated through the element u8ScanDuration, as described in the table below.
|
Action |
|---|---|
0x00-0x05 |
Perform radio channel scan on the set of channels specified through |
0x06-0xFD |
Reserved |
0xFE |
Change radio channel to single channel specified through |
0xFF |
Update the stored radio channel mask with that specified through |
The remote node replies with a Mgmt_NWK_Update_notify notification, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpMgmtNwkUpdateNotify(detailed in Section 9.2.3.41).
Parent topic:ZPS_eAplZdpMgmtNwkUpdateRequest
Parameters
hAPduInst Handle of APDU instance in which request is sent.
uDstAddr Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)
bExtAddr Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
* pu8SeqNumber Pointer to sequence number of request
* psZdpMgmtNwkUpdateReq Pointer to request (see above)
Parent topic:ZPS_eAplZdpMgmtNwkUpdateRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpMgmtNwkUpdateRequest
Parent topic:Network Management Services functions