ZPS_eAplZdpComplexDescRequest
ZPS\_teStatus ZPS\_eAplZdpComplexDescRequest\(
PDUM\_thAPduInstance hAPduInst,
ZPS\_tuAddress uDstAddr,
bool bExtAddr,
uint8 *pu8SeqNumber,
ZPS\_tsAplZdpComplexDescReq *psZdpComplexDescReq);
Description
This function requests the Complex descriptor of the node with a particular network address. The function sends a Complex_Desc_req request either to the relevant node or to another node that may hold the required information in its primary discovery cache.
The network address of the node of interest must be specified in the request, which is represented by the structure below (further detailed in Section 9.2.2.8).
typedef struct {
uint16 u16NwkAddrOfInterest;
} ZPS_tsAplZdpComplexDescReq;
The required Complex descriptor will be received in a Complex_Desc_rsp response, which should be collected using the function ZQ_bZQueueReceive() and stored in a structure of type ZPS_tsAplZdpComplexDescRsp(detailed in Section 9.2.3.7).
Parent topic:ZPS_eAplZdpComplexDescRequest
Parameters
hAPduInst: Handle of APDU instance in which request is sent
uDstAddr: Address of destination node of request (can be 16-bit or 64-bit, as specified by bExtAddr)
bExtAddr: Type of destination address:
TRUE: 64-bit IEEE (MAC) address
FALSE: 16-bit network address
*pu8SeqNumber: Pointer to sequence number of request
*psZdpComplexDescReq: Pointer to request (see above)
Parent topic:ZPS_eAplZdpComplexDescRequest
Returns
ZPS_E_SUCCESS (request successfully sent)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdpComplexDescRequest
Parent topic:Service Discovery functions