ZPS_eAplZdoRouteRequest#
ZPS_teStatus ZPS_eAplZdoRouteRequest(
uint16 u16DstAddr,
uint8 u8Radius);
Description#
This function requests the discovery of a route to the specified remote node (and that this route is added to the Routing tables in the relevant Router nodes).
Parent topic:ZPS_eAplZdoRouteRequest
Parameters#
u16DstAddr 16-bit network address of destination node
u8Radius Maximum number of hops permitted to destination node (zero value specifies that default maximum is to be used)
Parent topic:ZPS_eAplZdoRouteRequest
Returns#
ZPS_E_SUCCESS (route discovery request successfully initiated)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoRouteRequest
Parent topic:Routing functions