ZPS_eAplZdoManyToOneRouteRequest#
ZPS_teStatus ZPS_eAplZdoManyToOneRouteRequest(
bool bCacheRoute,
uint8 u8Radius);
Description#
This function requests a ‘many-to-one’ route discovery and should be called on a node that will act as a ‘concentrator’ in the network (that is, a node with which many other nodes will need to communicate).
As a result of this function call, a route discovery message is broadcast across the network and Routing table entries (for routes back to the concentrator) are stored in the Router nodes.
The maximum number of hops to be taken by a route discovery message in this broadcast must be specified. There is also an option to store the discovered routes in a Route Record Table on the concentrator (for return communications).
Parent topic:ZPS_eAplZdoManyToOneRouteRequest
Parameters#
bCacheRoute: Indicates whether to store routes in Route Record Table:
TRUE - store routes
FALSE - do not store routes
u8Radius: Maximum number of hops of route discovery message (zero value specifies that default maximum is to be used)
Parent topic:ZPS_eAplZdoManyToOneRouteRequest
Returns#
ZPS_E_SUCCESS (many-to-one route discovery successfully initiated)
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplZdoManyToOneRouteRequest
Parent topic:Routing functions