MCUXpresso SDK Documentation

ZPS_eAplAfUnicastIeeeDataReq

ZPS_eAplAfUnicastIeeeDataReq#

ZPS\_teStatus ZPS\_eAplAfUnicastIeeeDataReq(
        PDUM\_thAPduInstance hAPduInst,
        uint16 u16ClusterId,
        uint8 u8SrcEndpoint,
        uint8 u8DstEndpoint,
        uint64 u64DestAddr,
        ZPS\_teAplAfSecurityMode eSecurityMode,
        uint8 u8Radius,
        uint8 *pu8SeqNum);

Description#

This function submits a request to send data to a remote node (unicast), using the remote node’s IEEE (MAC) address. You must specify the local endpoint and output cluster from which the data originates (the cluster must be in the Simple descriptor for the endpoint), as well as the IEEE address of the remote node and the destination endpoint on the node.

The data is sent in an Application Protocol Data Unit (APDU) instance, which can be allocated using the PDUM function PDUM_hAPduAllocateAPduInstance() and then written to using PDUM_u16APduInstanceWriteNBO().

If the APDU size is larger than the maximum packet size allowed on the network, this function call will fail (and return ZPS_E_ADSU_TOO_LONG). To send large APDUs, use the function ZPS_eAplAfUnicastIeeeAckDataReq(), which automatically implements data fragmentation (if required).

Once the sent data has reached the first hop node in the route to its destination, a ZPS_EVENT_APS_DATA_CONFIRM event is generated on the local node.

If users try to send data using this function to a destination for which a route has not already been established, the data is not sent. Instead, a route discovery is performed. In this case, the function returns ZPS_NWK_ENUM_ROUTE_ERROR and must later be re-called to send the data (see Note under Section 6.5.1.1, “Unicast”).

Security (encryption/decryption) can be applied to the APDU, where this security can be implemented at the Application layer or the network (ZigBee) layer, or both.

Parent topic:ZPS_eAplAfUnicastIeeeDataReq

Parameters#

  • hAPduInst: Handle of APDU instance to be sent

  • u16ClusterId: Identifier of relevant output cluster on source endpoint

  • u8SrcEndpoint: Source endpoint number (1-240) on local node

  • u8DstEndpoint: Destination endpoint number (1-240) on remote node

  • u64DestAddr: IEEE (MAC) address of destination node

  • eSecurityMode: Security mode for data transfer:

    • ZPS_E_APL_AF_UNSECURE (no security enabled)

    • ZPS_E_APL_AF_SECURE (Application-level security using link key and network key)

    • ZPS_E_APL_AF_SECURE_NWK (Network-level security using network key)

    • ZPS_E_APL_AF_SECURE | ZPS_E_APL_AF_EXT_NONCE (Application-level security using link key and network key with the extended NONCE included in the frame)

    • ZPS_E_APL_AF_WILD_PROFILE (May be combined with above flags using OR operator. Sends the message using the wildcard profile (0xFFFF) instead of the profile in the associated Simple descriptor)

  • u8Radius: Maximum number of hops permitted to destination node (zero value specifies that default maximum is to be used)

  • *pu8SeqNum: Pointer to location to receive sequence number assigned to data transfer request. If not required, set to NULL

Parent topic:ZPS_eAplAfUnicastIeeeDataReq

Returns#

Parent topic:ZPS_eAplAfUnicastIeeeDataReq

Parent topic:Data Transfer functions