MCUXpresso SDK Documentation

ZPS_eAplAfUnicastDataReq

ZPS_eAplAfUnicastDataReq#

ZPS\_teStatus ZPS\_eAplAfUnicastDataReq\(
        PDUM\_thAPduInstance hAPduInst,
        uint16 u16ClusterId,
        uint8 u8SrcEndpoint,
        uint8 u8DstEndpoint,
        uint16 u16DestAddr,
        ZPS\_teAplAfSecurityMode eSecurityMode,
        uint8 u8Radius,
        uint8 *pu8SeqNum);

Description#

This function submits a request to send data to a remote node (unicast), using the remote node’s network address. You must specify the local endpoint and output cluster from which the data originates (the cluster must be in the Simple descriptor for the endpoint), as well as the network address of the remote node and the destination endpoint on the node.

The data is sent in an Application Protocol Data Unit (APDU) instance, which can be allocated using the PDUM function PDUM_hAPduAllocateAPduInstance() and then written to using PDUM_u16APduInstanceWriteNBO().

If the APDU size is larger than the maximum packet size allowed on the network, this function call will fail (and return ZPS_E_ADSU_TOO_LONG). To send large APDUs, use the function ZPS_eAplAfUnicastAckDataReq(), which automatically implements data fragmentation (if required).

Once the sent data has reached the first hop node in the route to its destination, a ZPS_EVENT_APS_DATA_CONFIRM event will be generated on the local node.

If data is sent using this function to a destination for which a route has not already been established, the data will not be sent and a route discovery will be performed instead. In this case, the function will return ZPS_NWK_ENUM_ROUTE_ERROR and must later be re-called to send the data (see Note under Section 6.5.1.1, “Unicast”).

Security (encryption/decryption) can be applied to the APDU, where this security can be implemented at the Application layer or the network (ZigBee) layer, or both.

Parent topic:ZPS_eAplAfUnicastDataReq

Parameters#

  • hAPduInst: Handle of APDU instance to be sent

  • u16ClusterId: Identifier of relevant output cluster on source endpoint

  • u8SrcEndpoint: Source endpoint number (1-240) on local node

  • u8DstEndpoint: Destination endpoint number (1-240) on remote node

  • u16DstAddr: Network address of destination node

  • eSecurityMode: Security mode for data transfer:

    • ZPS_E_APL_AF_UNSECURE (no security enabled)

    • ZPS_E_APL_AF_SECURE (Application-level security using link key and network key)

    • ZPS_E_APL_AF_SECURE_NWK (Network-level security using network key)

    • ZPS_E_APL_AF_SECURE | ZPS_E_APL_AF_EXT_NONCE (Application-level security using link key and network key with the extended NONCE included in the frame)

    • ZPS_E_APL_AF_WILD_PROFILE (May be combined with above flags using OR operator. Sends the message using the wildcard profile (0xFFFF) instead of the profile in the associated Simple descriptor)

  • u8Radius: Maximum number of hops permitted to destination node (zero value specifies that default maximum is to be used)

  • *pu8SeqNum: Pointer to location to receive sequence number assigned to data transfer request. If not required, set to NULL

Parent topic:ZPS_eAplAfUnicastDataReq

Returns#

Parent topic:ZPS_eAplAfUnicastDataReq

Parent topic:Data Transfer functions