ZPS_eAplAfGetEndpointDiscovery#
ZPS\_teStatus ZPS\_eAplAfGetEndpointDiscovery\(
uint8 u8Endpoint,
uint16 u16ClusterId,
bool bOutput,
bool\_t *pbDiscoverable);
Description#
This function obtains the discoverable state of the specified cluster of the specified endpoint on the local node - that is, whether the cluster/endpoint will be included in ‘device discoveries’ initiated on the network.
If the cluster/endpoint is discoverable, it appears in the Simple descriptor of the local node and is also included in match results requested using the function ZPS_eAplZdpMatchDescRequest().
The initial discoverable state of the cluster/endpoint is pre-set using the ZPS Configuration Editor (see Chapter 13). The state can subsequently be changed at runtime using the function ZPS_eAplAfSetEndpointDiscovery().
Parent topic:ZPS_eAplAfGetEndpointDiscovery
Parameters#
u8Endpoint: Endpoint number (on local node)
u16ClusterId: Cluster ID
bOutput: Type of cluster (output or input), one of:
TRUE: Output cluster
FALSE: Input cluster
*pbDiscoverable: Pointer to location to receive discoverable state, which is one of the below:
TRUE: Discoverable
FALSE: Not discoverable
Parent topic:ZPS_eAplAfGetEndpointDiscovery
Returns#
ZPS_E_SUCCESS
APS return codes, listed and described in Section 11.2.2
NWK return codes, listed and described in Section 11.2.3
MAC return codes, listed and described in Section 11.2.4
Parent topic:ZPS_eAplAfGetEndpointDiscovery
Parent topic:Endpoint functions