MCUXpresso SDK Documentation

ZPS Configuration Editor wizard

ZPS Configuration Editor wizard#

Before you can start to create a new ZigBee PRO stack configuration, the ZPS Configuration Editor plug-in must be installed in MCUXpresso.

To check if the plug-in is already installed, start MCUXpresso and select

File > New > Other from the main menu. Check that a Jennic option exists in the Select a Wizard dialogue box - expanding the Jennic option should show “ZBPro Configuration”, as illustrated in the screenshot below.

Selecting a Wizard

Using the wizard highlighted in the screenshot above, you can start to create a new ZigBee PRO configuration, as described in Section 12.4.1.

If the wizard is not present, install the ZPS Configuration Editor plug-in, which is supplied in the ZigBee 3.0 SDK.

Parent topic:ZPS Configuration Editor