MCUXpresso SDK Documentation

ZPS_bNwkFindAddIeeeAddr

ZPS_bNwkFindAddIeeeAddr#

bool_t ZPS_bNwkFindAddIeeeAddr(
                void *pvNwk,
                uint64 u64IeeeAddr,
                uint16 *pu16Location,
                bool_t bNeighborTable);

Description#

This function can be used to add the 64-bit IEEE (MAC) address of a node to the local MAC Address table. The function first searches the table to determine whether the address already exists in the table. If there is no entry for this address, a new entry for it is added to the table. The number of the entry where the address was found or added is returned in a specified location.

Note: You should modify the MAC Address table only using the supplied API functions and never write to it directly.

Parent topic:ZPS_bNwkFindAddIeeeAddr

Parameters#

  • pvNwk: Pointer to relevant NWK layer instance

  • u64IeeeAddr: 64-bit IEEE/MAC address to be added

  • pu16Location: Pointer to location to receive number of entry in MAC Address table where specified address was found or added

  • bNeighborTable: Always set to FALSE

Parent topic:ZPS_bNwkFindAddIeeeAddr

Returns#

Boolean indicating the outcome of the operation:

  • TRUE - address successfully added to the table

  • FALSE - address found to already exist in the table

Parent topic:ZPS_bNwkFindAddIeeeAddr

Parent topic:Addressing functions