MCUXpresso SDK Documentation

ZPS_bAplZdoTrustCenterRemoveDevice

ZPS_bAplZdoTrustCenterRemoveDevice#

ZPS_teStatus ZPS_bAplZdoTrustCenterRemoveDevice(
                            uint64 u64DeviceAddr);

Description#

This function can be used by the Trust Centre to delete a node in its information base.

Parent topic:ZPS_bAplZdoTrustCenterRemoveDevice

Parameters#

u64DeviceAddr : It is the 64-bit IEEE/MAC address of the node to be removed from the list.

Parent topic:ZPS_bAplZdoTrustCenterRemoveDevice

Returns#

  • ZPS_E_SUCCESS (node successfully removed from list)

  • APS return codes, listed and described in Section 11.2.2

  • NWK return codes, listed and described in Section 11.2.3

  • MAC return codes, listed and described in Section 11.2.4

Parent topic:ZPS_bAplZdoTrustCenterRemoveDevice

Parent topic:Security functions