ZigBee 3.0 SDK#
The ZigBee 3.0 SDK provides the stack and API software resources needed to develop ZigBee 3.0 applications for the JN518x and K32W041/K32W061/K32W1/MCXW71/MCXW72/RW612 devices and includes:
ZigBee PRO and IEEE 802.15.4 stack software
ZigBee PRO APIs
ZigBee Base Device Behavior (BDB) APIs
ZigBee Cluster Library (ZCL) APIs
Connectivity Framework APIs
ZPS Configuration Editor
Integrated Peripherals APIs and Board APIs
NXP-specific tools have been devised for MCUXpresso, including the ZPS Configuration Editor, which is provided as an Eclipse plug-in. This tool is used to set network parameters and is described in Chapter 13, ZPS Configuration Editor.
This ZigBee 3.0 SDK contains device-specific plug-ins for the MCUXpresso platform.
MCUXpresso must be installed before the ZigBee 3.0 SDK. Refer to Section 5.1.1, Development platform for information on this toolchain.
Parent topic:Development environment and resources