MCUXpresso SDK Documentation

References

References#

For more information, refer to the following documents:

  • Bluetooth Low Energy Application Developer’s Guide (KW47_BLEADG)

  • Bluetooth Low Energy Host Stack API Reference Manual (KW47_BLEHSAPIRM)

  • Bluetooth Low Energy Host Stack FSCI (Framework Serial Connectivity Interface) API Reference Manual(KW47_BLEHSFSCIRM)

  • Connectivity Framework Reference Manual (KW47_CONNFWRM)

  • Bluetooth Low Energy CCC Digital Key R3 Application Note (AN12791)

Refer to the the below specifications: