MCUXpresso SDK Documentation

Memory requirements

Memory requirements#

The following are the memory requirements for the SSRC module.

Memory item

Size in bytes

Instance memory (persistent)

548

Scratch memory (non-persistent)

15.536 1

Program memory for Arm9E and XScale

14k

Program memory for Arm7

15k

Parent topic:Resource usage

1 Worst case number for I/O buffers of 40 ms. If smaller I/O buffers are used, this number is smaller. The required scratch memory is roughly equal to 2 times the buffer size on the highest sample rate.