Hardware requirements#
Mini/micro USB cable
MCX-N9XX-EVK Board
Personal Computer
TFT Proto 5” CAPACITIVE board HW REV 1.01 by Mikroelektronika.
Board settings#
Connect the panel to header J20. Pin 1 match Pin 1.
Prepare the Demo#
Connect a USB cable between the host PC and the EVK board J5.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When the project running, the panel shows as overview described.