MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • IMX95VERDIN-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings#

No special settings are required.

Please note this application can’t support running with Linux BSP!

Prepare the Demo#

  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch S6 to power on the board.

  2. Connect a micro USB cable between the host PC and the J4 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo#

When the demo runs successfully, will get the similar messages on the terminal.

 Timestamp1 = 01c98d6

 Test the delay function, delay for 1 second

 Start time = 01cb123

 End time = 02bfbd3