Hardware requirements#
Micro USB cable
two IMX95LPD5-EVK board
JLink Plus
12V~20V power supply
Personal Computer
Board settings#
The example requires connecting between CAN pins of two boards. The connection should be set as follows:
Between two boards:
J17-2(CANH) node A, J17-2(CANH) node B
J17-3(CANL) node A, J17-3(CANL) node B
J17-4(GND) node A, J7-4(GND) node B
Prepare the Demo#
Connect 12V~20V power supply and JLink Plus to the board, switch SW4 to power on the board
Connect a micro USB cable between the host PC and the J31 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
When setting ENABLE_LOOPBACK macro and the example runs successfully, you can see the similar information from the terminal as below.
FlexCAN Enhanced Rx FIFO edma example.
Loopback mode, Message buffer 0 used for Tx, Enhanced Rx FIFO used for Rx.
Press any key to trigger 4 transmission.
Send Msg0 to Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, id = 0x123.
Send Msg1 to Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, id = 0x124.
Send Msg2 to Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, id = 0x125.
Send Msg3 to Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, id = 0x126.
Receive Msg0 from Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, ID Filter Hit: 0, Time stamp: 41410.
Receive Msg1 from Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, ID Filter Hit: 1, Time stamp: 48882.
Receive Msg2 from Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, ID Filter Hit: 2, Time stamp: 56352.
Receive Msg3 from Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, ID Filter Hit: 3, Time stamp: 63821.
Press any key to trigger 4 transmission.
...
==FlexCAN loopback functional example – Start.==
2 boards are required to be connected through CAN bus if ENABLE_LOOPBACK is not defined. One board must be chosen as node A and the other board as node B. (Note: Node B should start first) Data is sent continuously between the node A and the node B.
This message displays on the node A terminal:
FlexCAN Enhanced Rx FIFO edma example.
Board to board mode.
Node B Enhanced Rx FIFO used for Rx.
Node A Message buffer 0 used for Tx.
Please select local node as A or B:
Note: Node B should start first.
Node:a
Press any key to trigger 4 transmission.
Send Msg0 to Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, id = 0x123.
Send Msg1 to Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, id = 0x124.
Send Msg2 to Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, id = 0x125.
Send Msg3 to Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, id = 0x126.
Press any key to trigger 4 transmission.
....
This message displays on the node B terminal:
FlexCAN Enhanced Rx FIFO interrupt example.
Board to board mode.
Node B Enhanced Rx FIFO used for Rx.
Node A Message buffer 0 used for Tx.
Please select local node as A or B:
Note: Node B should start first.
Node:b
Start to Wait data from Node A.
Receive Msg0 from Enhanced Rx FIFO: word0 = 0x0, word1 = 0x55, ID Filter Hit: 0, Time stamp: 24286.
Receive Msg1 from Enhanced Rx FIFO: word0 = 0x1, word1 = 0x55, ID Filter Hit: 1, Time stamp: 25059.
Receive Msg2 from Enhanced Rx FIFO: word0 = 0x2, word1 = 0x55, ID Filter Hit: 2, Time stamp: 25745.
Receive Msg3 from Enhanced Rx FIFO: word0 = 0x3, word1 = 0x55, ID Filter Hit: 3, Time stamp: 26431.
Wait for the next 4 messages!
....