Hardware requirements#
Type-Micro USB cable
FRDM-KE17Z512 board
Personal Computer
Overview#
This application demonstrates use of certified NXP Safety Library 5.0 which meets the IEC60730 class B standard.
More information#
More information about the Safety Library with the board specific Library/Example User’s guide, release note, certificate and other documentation: http://www.nxp.com/iec60730
Board settings#
Follow chapter “Hardware setup” in Example User’s guide.
Running the demo#
Follow chapter “Running example” in Example User’s guide.