Hardware requirements#
Mini/micro USB cable
MIMXRT1180-EVK board
Personal Computer
Board settings#
For MCUX IDE, erase the flash with SW5=0000, as noted in the Getting started guide, then set SW5=0100.
Prepare the Demo#
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo#
The log below shows the output of the hello world demo in the terminal window:
mbedTLS version 2.28.5
fsys=240000000
Using following implementations:
SHA: Software implementation
AES: ELE S40x HW accelerated
AES GCM: Software implementation
DES: Software implementation
Asymmetric cryptography: ELE S40x HW accelerated RSA
MD5 : 474.13 KiB/s, 487.46 cycles/byte
SHA-1 : 607.04 KiB/s, 379.35 cycles/byte
SHA-256 : 1819.17 KiB/s, 121.53 cycles/byte
SHA-512 : 1667.46 KiB/s, 133.48 cycles/byte
AES-CBC-128 : 2662.44 KiB/s, 80.72 cycles/byte
AES-CBC-192 : 2654.76 KiB/s, 80.97 cycles/byte
AES-CBC-256 : 2647.99 KiB/s, 81.19 cycles/byte
AES-XTS-128 : 79.08 KiB/s, 2993.83 cycles/byte
AES-XTS-256 : 78.51 KiB/s, 3016.67 cycles/byte
AES-GCM-128 : 48.20 KiB/s, 4955.88 cycles/byte
AES-GCM-192 : 48.09 KiB/s, 4967.43 cycles/byte
AES-GCM-256 : 47.97 KiB/s, 4982.34 cycles/byte
AES-CCM-128 : 3219.24 KiB/s, 65.46 cycles/byte
AES-CCM-192 : 2899.25 KiB/s, 73.51 cycles/byte
AES-CCM-256 : 2637.28 KiB/s, 81.51 cycles/byte
AES-CMAC-128 : 78.23 KiB/s, 3026.06 cycles/byte
AES-CMAC-192 : 77.92 KiB/s, 3037.69 cycles/byte
AES-CMAC-256 : 77.57 KiB/s, 3052.74 cycles/byte
AES-CMAC-PRF-128 : 78.13 KiB/s, 3030.14 cycles/byte
Poly1305 : 481.49 KiB/s, 480.18 cycles/byte
BLOWFISH-CBC-128 : 187.46 KiB/s, 1249.64 cycles/byte
BLOWFISH-CBC-192 : 187.46 KiB/s, 1249.63 cycles/byte
BLOWFISH-CBC-256 : 187.46 KiB/s, 1249.66 cycles/byte
CTR_DRBG (NOPR) : 82.48 KiB/s, 2865.79 cycles/byte
CTR_DRBG (PR) : 62.09 KiB/s, 3825.00 cycles/byte
HMAC_DRBG SHA-1 (NOPR) : 39.88 KiB/s, 6019.47 cycles/byte
HMAC_DRBG SHA-1 (PR) : 36.99 KiB/s, 6503.91 cycles/byte
HMAC_DRBG SHA-256 (NOPR) : 20.72 KiB/s, 11865.59 cycles/byte
HMAC_DRBG SHA-256 (PR) : 20.72 KiB/s, 11865.89 cycles/byte
RSA-2048 : 7.33 private/s
RSA-2048 : 419.33 public/s