MCUXpresso SDK Documentation

MCUXpresso Config Tools

MCUXpresso Config Tools#

MCUXpresso Config Tools can help configure the processor and generate initialization code for the on chip peripherals. The tools are able to modify any existing example project, or create a new configuration for the selected board or processor. The generated code is designed to be used with MCUXpresso SDK version 2.x.

Table 1 describes the tools included in the MCUXpresso Config Tools.

Config Tool

Description

Image

Pins tool

For configuration of pin routing and pin electrical properties.​

| |Clock tool|For system clock configuration|

| |Peripherals tools|For configuration of other peripherals|

| |TEE tool|Configures access policies for memory area and peripherals helping to protect and isolate sensitive parts of the application.​|

| |Device Configuration tool|Configures Device Configuration Data (DCD) contained in the program image that the Boot ROM code interprets to setup various on-​chip peripherals prior the program launch.​|

|

MCUXpresso Config Tools can be accessed in the following products:

  • Integrated in the MCUXpresso IDE. Config tools are integrated with both compiler and debugger which makes it the easiest way to begin the development.

  • Standalone version available for download from www.nxp.com/mcuxpresso. Recommended for customers using IAR Embedded Workbench, Keil MDK µVision, or Arm GCC.

  • Online version available on mcuxpresso.nxp.com. Recommended to do a quick evaluation of the processor or use the tool without installation.

Each version of the product contains a specific Quick Start Guide document MCUXpresso IDE Config Tools installation folder that can help start your work.