MCUXpresso SDK Documentation

Hardware requirements#

  • Micro USB cable

  • IMX952LPD5EVK-19 board

  • J-Link Debug Probe

  • 12V~20V power supply

  • MX9_LVDS_LD panel

  • Personal Computer

Board settings#

For MX9_LVDS_LD panel(1920*720), connect MINISAS ports J15 and J16 to panel.

Prepare the Demo#

  1. Connect 12V power supply and J-Link Debug Probe to the board, switch SW4 to power on the board.

  2. Connect a micro USB cable between the host PC and the J31 USB port on the cpu board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Launch the debugger in your IDE to begin running the example.

Steps to configure the panels#

Default panel is MX9_LVDS_LD panel, default port is DPU_DI_LVDS, default setting for APP_DISPLAY_EXTERNAL_CONVERTOR is disabled Tips: The APP_DISPLAY_EXTERNAL_CONVERTOR can be set as 1 when you are using MIPI2HDMI card(ADV7535) or LVDS2HDMI card(IT6263) only. When Kconfig is used#

Below setting is for kconfig, the settings in dpu/localdimming/cm7/prj.conf For default MX9_LVDS_LD panel, you do not need to change anything. When package is used#

Below setting is for mcux_config.h. For default MX9_LVDS_LD panel, Setting DEMO_PANEL to 18. You also need to set LDB_DUAL_PANEL to 1.

Running the demo#

When the example runs successfully, you can see the rectangles and diamonds shown in the screen.