Hardware requirements#
Mini/micro USB cable
EVKB-IMXRT1050 board
Personal Computer
Oscilloscope
Board settings#
weld resister 0Ω at R279 R280 R281.
Probe the pwm signal using an oscilloscope
At J24-3
At J24-4
At J24-6
At TP27
Prepare the Demo#
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo#
When the example runs successfully, the following message is displayed in the terminal:
FlexPWM driver example
~~~~~~~~~~~~~~~~~~~~~~~