Compiler/Debugger#
The MCUXpresso SDK i.MX 93 release supports building and debugging with the toolchains listed in Table 1.
The user can choose the appropriate one for development.
For supported toolchain versions, see MCUXpresso SDK Release Notes for MCIMX93-QSB (document: MCUXSDKMCIMX93QSBRN).
Arm GCC + SEGGER J-Link GDB Server. This is a command line tool option and it supports both Windows OS and Linux OS.
IAR Embedded Workbench for Arm and SEGGER J-Link software. The IAR Embedded Workbench is an IDE integrated with editor, compiler, debugger, and other components. The SEGGER J-Link software provides the driver for the J-Link Plus debugger probe and supports the device to attach, debug, and download.
Compiler/Debugger |
Supported host OS |
Debug probe |
Tool website |
|---|---|---|---|
ArmGCC/J-Link GDB server |
Windows OS/Linux OS |
J-Link Plus |
| |IAR/J-Link|Windows OS|J-Link Plus|www.iar.com
|
Download the corresponding tools for the specific host OS from the website.
Note:
To support i.MX 93, the patch for IAR and Segger J-Link must be installed. To download, navigate to https://www.nxp.com/webapp/Download?colCode=SDK_MX93_3RDPARTY_PATCH&appType=license)).
Parent topic:Toolchain introduction