Version 2.1.2#
New features#
Mbed TLS upgrade to v3.6.3.
New platforms supported#
Hotfixes#
Protected Storage content can be lost if the storage is “full”, psa_ps_set is attempted and device is reset (twice).
Fix wrapper to properly mark NSPE images as such
SPM: Remove specific section for psa_interface_thread_fn_call
SPM: interrupts: Add missing checks on fih_rc return value
SPM: Services do not unmap IOVECS
SPM: SPM does not return PSA_ERROR on refused psa_connect
SPM: Fixes for invalid connection retention after psa_close
SPM: Fixes for reverse-handle
Known issues#
Some open issues are not fixed in this release.
Descriptions |
Issue links |
|---|---|
SPM does not automatically unmap mm-iovecs. |
SPDX-License-Identifier: BSD-3-Clause
SPDX-FileCopyrightText: Copyright The TrustedFirmware-M Contributors