MCUXpresso SDK Documentation

MAX32657#

Introduction#

The MAX32657 microcontroller (MCU) is an advanced system-on-chip (SoC) featuring an Arm® Cortex®-M33 core with single-precision floating point unit (FPU) with digital signal processing (DSP) instructions, large flash and SRAM memories, and the latest generation Bluetooth® 5.4 Low Energy (LE) radio. The nano-power modes increase battery life substantially.

MAX32657 1MB flash and 256KB RAM split to define section for MCUBoot, TF-M (S), Zephyr (NS) and storage that used for secure services and configurations. Default layout of MAX32657 is listed in below table.

Name

Address[Size]

Comment

boot

0x1000000[64K]

MCU Bootloader

slot0

0x1010000[320k]

Secure image slot0 (TF-M)

slot0_ns

0x1060000[576k]

Non-secure image slot0

slot1

0x10F0000[0k]

Updates slot0 image

slot1_ns

0x10F0000[0k]

Updates slot0_ns image

storage

0x10f0000[64k]

File system, persistent storage

RAM

Address[Size]

Comment

secure_ram

0x30000000[64k]

Secure memory

non_secure_ram

0x20010000[192k]

Non-Secure memory

Secure Boot ROM#

MAX32657 has Secure Boot ROM that used to authenticate user code via ECDSA 256 public key. The Secure Boot ROM is disabled on default, to enable it user need to provision device first.

ADI provides enable_secure_boot.py (under <CMAKE_BINARY_DIR>/lib/ext/tesa-toolkit-src/devices/max32657/scripts/bl1_provision) script to simply provision the device. This script reads user certificate via command line parameter then writes user key on the device and disables debug interface.

To create pub & private key pair for MAX32657 run:

openssl ecparam -out <MY_CERT_FILE.pem> -genkey -name prime256v1

Note

Debug interface will be disabled after secure boot is enabled. User must write final firmware before provisioning the device. It can be written during device provision, Just add your final firmware hex file in JLinkScript under <CMAKE_BINARY_DIR>/lib/ext/tesa-toolkit-src/devices/max32657/scripts/bl1_provision folder.

After secure boot has been enabled BL2 image must be signed with user certificate otherwise Secure Boot ROM will not validate BL2 image and will not execute it. The sign process will be done automatically if BL1 be ON -DBL1=ON The sign key can be sepecified over command line option -DTFM_BL2_SIGNING_KEY_PATH=<MY_KEY_FILE> or by setting the flag in <TF-M base folder>/platform/ext/target/adi/max32657/config.cmake Development purpose test certificate is here: <CMAKE_BINARY_DIR>/lib/ext/tesa-toolkit-src/devices/max32657/keys/bl1_dummy.pem It shall not been used for production purpose just for development purpose.

Note

The signature generation depends on ecdsa that’s have to be installed:

pip3 install ecdsa

Building TF-M#

This platform port supports TF-M regression tests (Secure and Non-secure) with Isolation Level 1.

To build S and NS application, run the following commands:

Note

Only GNU toolchain is supported.

Note

Only “profile_small” predefined profile is supported.

Prepare the tf-m-tests repository inside the TF-M base folder.

cd <TF-M base folder>
git clone https://git.trustedfirmware.org/TF-M/tf-m-tests.git
cd <TF-M base folder>/tf-m-test/tests_reg

cmake -S spe -B build_spe \
        -G"Unix Makefiles"               \
        -DTFM_PLATFORM=adi/max32657      \
        -DCONFIG_TFM_SOURCE_PATH=<TF-M base folder>/trusted-firmware-m \
        -DTFM_TOOLCHAIN_FILE=<TF-M base folder>/trusted-firmware-m/toolchain_GNUARM.cmake \
        -DTEST_S=OFF                \
        -DTEST_NS=ON               \
        -DTFM_NS_REG_TEST=ON        \
        -DMCUBOOT_LOG_LEVEL="INFO"  \
        -DTFM_ISOLATION_LEVEL=1
cmake --build build_spe -- install

cmake -S . -B build_test    \
        -G"Unix Makefiles"  \
        -DCONFIG_SPE_PATH=<TF-M base folder>/tf-m-tests/tests_reg/build_spe/api_ns \
        -DTFM_TOOLCHAIN_FILE=cmake/toolchain_ns_GNUARM.cmake \
        -DTFM_NS_REG_TEST=ON
cmake --build build_test

Merge and Flash Images#

Follow the steps below to program the flash with a compiled TF-M image (i.e. S, NS or both).

Generate Intel hex files from the output binary (bin) files as follows:

srec_cat build_test/bin/tfm_ns_signed.bin -binary --offset 0x01060000 -o build_test/bin/tfm_ns_signed.hex -intel

Merge hex files as follows:

srec_cat.exe build_spe/bin/bl2.hex -Intel build_spe/bin/tfm_s_signed.hex -Intel build_test/bin/tfm_ns_signed.hex -Intel -o tfm_merged.hex -Intel

Note

Use bl2_signed.hex instead bl2.hex if Secure Boot ROM is enabled.

Flash them with JLink as follows:

JLinkExe -device MAX32657 -if swd -speed 2000 -autoconnect 1
J-Link>h
J-Link>r
J-Link>erase
J-Link>loadfile build_spe/bin/tfm_merged.hex

BL2 and TF-M Provisioning#

On default -DPLATFORM_DEFAULT_PROVISIONING=ON and -DTFM_DUMMY_PROVISIONING=ON which will use default provisioning and dummpy keys, these configuration is fine for development purpose but for production customer specific keys shall be used Provisioning bundles can be generated with the -DPLATFORM_DEFAULT_PROVISIONING=OFF flag. The provisioning bundle binary will be generated and it’s going to contain the provisioning code and provisioning values.

If -DPLATFORM_DEFAULT_PROVISIONING=OFF and -DTFM_DUMMY_PROVISIONING=ON then the keys in the tf-m/platform/ext/target/common/provisioning/provisioning_config.cmake and the default MCUBoot signing keys will be used for provisioning.

If -DPLATFORM_DEFAULT_PROVISIONING=OFF and -DTFM_DUMMY_PROVISIONING=OFF are set then unique values can be used for provisioning. The keys and seeds can be changed by passing the new values to the build command, or by setting the -DPROVISIONING_KEYS_CONFIG flag to a .cmake file that contains the keys. An example config cmake file can be seen at tf-m/platform/ext/target/common/provisioning/provisioning_config.cmake. Otherwise new random values are going to be generated and used. For the image signing the ${MCUBOOT_KEY_S} and ${MCUBOOT_KEY_NS} will be used. These variables should point to .pem files that contain the code signing private keys. The public keys are going to be generated from these private keys and will be used for provisioning. The hash of the public key is going to be written into the provisioning_data.c automatically.

If -DMCUBOOT_GENERATE_SIGNING_KEYPAIR=ON is set then a new mcuboot signing public and private keypair is going to be generated and it’s going to be used to sign the S and NS binaries.

The new generated keypair can be found in the <build dir>/bin folder or in the <install directory>/image_signing/keys after installation. The generated provisioning_data.c file can be found at <build directory>/platform/target/provisioning/provisioning_data.c

Note

The provisioning bundle generation depends on pyelftools that’s have to be installed:

pip3 install pyelftools

UART Console#

MAX32657 has one UART (UART0) peripheral which is routed for Non-Secure console output by default. S and NS firmware can not use UART at the same time. If TFM_S_REG_TEST been defined the UART console will be routed to the Secure side otherwise it will be on NS side.


Copyright 2025 Analog Devices, Inc. All rights reserved. *SPDX-License-Identifier: BSD-3-Clause